Browse FAQs

What is the difference between Observers and Supervisors inside Dashboards in PME?

Published date: 20 May 2019

Product Line
Power Monitoring Expert

Environment
User Manager

Resolution
In the Web Application Dashboard, Observers are only able to see what is available without the ability to edit or control.

Supervisors are able to edit and control current dashboards and create new diagrams. Also, if they make a Dashboard private, Observers cannot see it.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.