Browse FAQs

Are AccuSine devices monitored in Power Quality Advisor natively?

Published date: 15 March 2019

Issue   
Need to know when running a Power Quality Advisor gadget/report will the AccuSine devices be part of it?

Product Line      
PME 8.2 
PME 9.0
AccuSine PCS
AccuSine PCS+
AccuSine PFV+

Resolution
In PME 8.2 and above the below AccuSine products have native drivers -
- AccuSine PCS
- AccuSine PCS Plus
- AccuSine PFV Plus 

As per the PQ Advisor Design Guide, in PME we have Standardized Equipment Diagrams for the below products(Hence below products are Native & can monitor the same in PME):
- AccuSine PCS Plus
- AccuSine PFV Plus 

Note: The corrective equipment diagrams are developed to support the products listed above. If the user’s corrective equipment is not in the above list, the application engineer can modify the default diagrams to work with the equipment, or create custom diagram pages for it.

For more details refer the PQ Advisor Design Guide and below is the link for the same.
https://www.schneider-electric.com/resources/sites/SCHNEIDER_ELECTRIC/content/live/FAQS/291000/FA291129/en_US/PQAdvisor%20Design%20Guide%207EN42-0164-00.pdf

Link for PQ Advisor Configuration Guide.pdf ->
http://www2.schneider-electric.com/resources/sites/SCHNEIDER_ELECTRIC/content/live/FAQS/291000/FA291129/en_US/PQAdvisor_Configuration_Guide.pdf

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.