Technical FAQs

Ask a Question

What are the different web browser supported by ClearSCADA 2017?

Web Browser Support

ClearSCADA's web interface, WebX, uses Microsoft’s ActiveX Controls technology to display Mimics, Lists, Trends, and so on. ActiveX Controls are only supported by Microsoft Internet Explorer; as such, the WebX client supports the 32-bit version of:

  • Internet Explorer 10
  • Internet Explorer 11.

(ClearSCADA's Original WebX client also supports Internet Explorer 8 and Internet Explorer 9.) 

Was this helpful?
What can we do to improve the information ?