Technical FAQs

Ask a Question

Osisense XU_Reliability data of the XUX0AKSAM12 photoelectric sensor MTTF ...

The reliability data of the XUX0AKSAM12 photoelectric sensor, multimode, are the following :
- MTTF = 1075 years (mean time to failure),
- MTTFD = 
2150 years (mean time to dangerous failure),
- DC = 0 (diagnostic coverage) of the sensor alone,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level).
The MTTF calculation is made according to the IEC 62380 standard, value for 30°C temperature.
Was this helpful?
What can we do to improve the information ?