Technical FAQs

Ask a Question

Osisense XZ - Is the XZBWE112A24 transmitter compatible with the ZBRRA or ZBRRD or ZBRRC programmable receiver?

The XZBWE112A24 transmitter is compatible with the XZBWR2STT24 receiver only. Refer to the attachment

Was this helpful?
What can we do to improve the information ?