Technical FAQs

Ask a Question

Preventa XY2C - In the XY2CED double sided rope pull switch, can we use a cable with a 3.2mm outer diameter, instead of 5mm recommended?

A 3.2mm cable would have more elasticity, which is favorable in terms of tripping by cable breakage, BUT we wouldn’t satisfy the limit values for the tripping deflection demanded by the CE/IEC 60947-5-5 standard, in the XY2CED rope pull switch installation.

Was this helpful?
What can we do to improve the information ?