Technical FAQs

Ask a Question

Preventa XY2C - Can we mount the XY2CED with a cable on one side only?

 No. Unlike the XY2CE rope pull switch, there is no internal spring inside the XY2CED double sided rope pull switch. The product architecture thus requires an end-spring on both sides to allow the cam motion when the cable is pulled.
Was this helpful?
What can we do to improve the information ?