Technical FAQs

Ask a Question

Can you use a potentiometer with an ATS22 or ATS48 Soft starter?

Issue:
Can you use a potentiometer with an ATS22 or ATS48 Sof tstarter?

Product Line:
Altistart 22, Altistart 48, or Solid State Starter

Environment:
All

Cause:
Speed adjustment

Resolution:
The ATS48 and ATS22 soft starters doe not have any speed control so there is no option to use a speed potentiometer on the soft starters. 
Was this helpful?
What can we do to improve the information ?