Technical FAQs

Ask a Question

Certificate of Conformity for ATEX environment for XB4***EX

 See certificate of conformity in attachment stating that the products are conform to EN 60079-31 ed2014.
It is based on the following:
- Schneider supplies operators and contacts to Ex-Tech who manufactures the Atex range
- Ex-Tech has the updated Ineris certificate  for their Dust + gaz version (Ineris 02ATEX9007U)
- The operator used for Ex-Tech range is the same than the one used for XB4***EX products. Only the contact is specific
- For dust certification, only the operator is considered. The contact is insulated in a control station
--> The EN 60079-31 ed2014 is applicable to Schneider Atex references
The official certificate from Ineris will be available first quarter 2018
Was this helpful?
What can we do to improve the information ?