Technical FAQs

Ask a Question

What are the Environmental characteristics of EM6400NG meters ?

Environmental characteristics

Operating temperature                -10 °C to +60 °C (14 °F to 140 °F)
Storage temperature                   -25 °C to +70 °C (-13 °F to 158 °F)
Humidity rating                           5% to 95% RH at 50 °C (122 °F) (non-condensing)
Pollution degree                          2
Altitude                                      < 2000 m (6562 ft)
Location                                    Not suitable for wet locations
Product life                               > 7 years
Was this helpful?
What can we do to improve the information ?