Technical FAQs

Ask a Question

What are the mechanical characteristics of EM6400NG meter ?

Mechanical characteristics:

IP degree of protection (IEC 60529-1)         Front display: IP51
                                                               Meter body: IP30
Panel thickness maximum                         6.0 mm (0.25 in) maximum
Mounting position                                      Vertical
Display type                                              LED display — 7 Segment
Keypad                                                     3 button
Front panel LED indicators                        Green LED (heartbeat / serial communications activity)
                                                               Red LED (energy pulse output)
Weight                                                    ~ 600 gms
Dimensions W x H x D                             96 x 96 x 73 mm max
Was this helpful?
What can we do to improve the information ?