Browse FAQs

What is the factory default ESIM output scaling of the PTO signal on Lexium 32?

Published date: 17 January 2019

The factory default setting of the PTO output of the ESIM signal is set at 4096 counts per revoultion.

The scaling is freely adjustable from 8 counts per revolution to 65535 counts per revolution.


rev 1-17-19

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.