Browse FAQs

What are the Unity DTM Browser Device properties settings?

Published date: 30 September 2019


Title
Unity DTM Browser Device properties settings
 
Issue
Unity DTM Browser settings
 
Product Line
M580 M340
 
Environment
Unity DTM Browser
 
Resolution
 The 'Items Management' in the Unity DTM Browser Device properties tab is used to created the Device DDT sub-element variables for a particular device.
The 'Re-import Items' button will put the Device DDT sub-element variables back to their default value or if using an enumerated EDS file, set the Device DDT sub-element variables to the EDS enumerated values. Setting the Item Management to Manual allows the user to manually changes tag names. After setting to Manual, Select the word "Items" under the device entry to manually changes your tag names. You will need to delete any existing individual tag element to then create a new element tag name.
The Connection Bit value is used as a tracking mechanism in Unity program. In a M580 program we recommend using the Freshness bits as your connection status bit.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.