Technical FAQs

Ask a Question

How to hide the FactoryCast banner for the PLC Program Viewer

Title
FactoryCast PLC Program Viewer 
 
Issue
FactoryCast PLC Program Viewer 
 
Product Line
FactoryCast 
 
Environment
FactoryCast
 
Cause
N/A
 
Resolution 
To configure the parameters in the URL to show or hide the PLC Program Viewer
-  navigation tree (at the left of the PLC program viewer), to show or
-  hide the console (at the bottom of the PLC program viewer), and to focus on a specific section or object in the PLC program.
-  Log in to the FactoryCast web site and use these URLs:
-  • Hide the FactoryCast banner:
               http://<IP>/#monitoring/plcpv?standalone=1
-  View a single section:
-             http://<IP>/#monitoring/plcpv?showTreeview=0&showConsole=0&section=<SECTION_NAME>&standalone=1
>
Note:  If security is enabled, you have to login first and then type the URL.

The changes are scheduled to be added to the help for Unity 14.
 
 
Was this helpful?
What can we do to improve the information ?