Technical FAQs

Ask a Question

L140 cable pull switch - Cross of the L1441M or L1443M cable pull switch

In 2017, the 3 references of cable pull switch L1441M, L1443M, L1444M are discontinued. They can be replaced by the alone reference available to order L1442M. The difference between the 4 references is the "base plate" only. The L1442M uses the style 2 base plate. They are supplied without any lever arm.

   
Was this helpful?
What can we do to improve the information ?