Technical FAQs

Ask a Question

Video: How to access the BMENOC0301 DTM Browser Diagnosis Window

Issue
Enabling access to the BMENOC0301 Modicon M580 Ethernet communication module's DTM (data type manager) Browser Diagnosis Window via Unity Pro.
 
Product Line
BMENOC0301
 
Environment
Unity Pro 12
 
Resolution
This video explains step by step how to access the BMENOC0301 DTM Browser Diagnosis Window. The BMENOC0301 DTM Browser Diagnosis Window will display the status of the remote device connections configured for the BMENOC0301 module.

 
Was this helpful?
What can we do to improve the information ?