Technical FAQs

Ask a Question

How to simulate an analog input with Unity

Unity Pro offers the Write _Input_Int block which can be used to accomplish either task.
The video linked to this FAQ will demonstrate this functionality using an M340. The information
is also valid for M580 and Quantum PLC's


 
Was this helpful?
What can we do to improve the information ?