Technical FAQs

Ask a Question

Osisense XC - Reliability data of the XCMN2102L* limit switch series like B10D

The reliability data of the XCMN plastic limit switch series, are the following :
- B10 = 5 millions operating cycles,
- B10D = 25 millions operating cycles for the NC contact and head positive,
- DC = 0 (diagnostic coverage) of the switch alone,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level).
Please note that a flexible operator head (example cat'whisker) cannot be used in a safety function (head not positive).
Was this helpful?
What can we do to improve the information ?