Technical FAQs

Ask a Question

What is Ics value in case cascading of circuit breakers

The cascading is managed by the Annex A of IEC 60947-2 standard and concerns only the Icu performances = "reinforced breaking capacity"
We don't test and we don't have any information on equivalent Ics value in cascading.
Was this helpful?
What can we do to improve the information ?