Technical FAQs

Ask a Question

Video: What parameter settings are needed for Lexium 28 being used as a rotary axis to make a homing movement?

When used as a rotary axis, in order for a Lexium 28 servo drive to properly perform a homing movement, it is necessary to have the proper I/O assignment.
It is not permitted to only assign a reference switch for a homing movement to function. LIMP and LIMN must also be assigned.

The following video demonstrates this procedure:

Was this helpful?
What can we do to improve the information ?