Technical FAQs

Ask a Question

Is Iconics compatible with Windows10?

Title:
Is Iconics compatible with Windows10?

Issue:
Customer was using Iconics with PME on a Windows 2012 Operating system without any problems.
a new computer with Windows10 is being used to access the Web Applications, all the web apps worked OK except Iconics.

Product Line:
Power Monitor Expert
Iconics

Environment:
Windows10 Operating System

Cause:
Unable to access Iconics from a Windows10 computer

Resolution:
Check the Iconics version to make sure it is compatible with Windows10 Operating System.
Below is the information on the Iconics versions that are compatible with Windows10 OS.

 ICONICS is a globally managed Microsoft Gold Partner and winner of the 2014 Microsoft Public Sector CityNext Partner of the Year award.
It provides advanced, Web-enabled and OPC UA certified HMI/SCADA and Analytics software for any discrete manufacturing or industrial application.
ICONICS announces that their latest 64-bit suites (the upcoming V10.9 versions of GENESIS64™, AnalytiX
®, Hyper Historian™,
and MobileHMI™) and 32-bit suites (the upcoming V9.4 versions of GENESIS32™ and BizViz™) will all be Windows 10 compatible.





 
Was this helpful?
What can we do to improve the information ?