Technical FAQs

Ask a Question

With which Acti9 circuit breakers is the PowerTag compatible?

The PowerTag modules are compatible with the following devices: single terminal circuit breakers and switches at intervals of 18mm, current ratings up to 63A.
The attached file contains the compatibility table between PowerTag and Acti9 / Multi9 devices.
Was this helpful?
What can we do to improve the information ?