Technical FAQs

Ask a Question

Osisense XG - UL 94 flammability rating of the network "T" connector M12 5-pin TCSCTN011M11F

UL 94 flammability rating of the network "T" connector M12 5-pin TCSCTN011M11F = HB
Was this helpful?
What can we do to improve the information ?