Technical FAQs

Ask a Question

What is the screw size that comes in the VW3A1006 remote keypad kit?

Issue:
What is the screw size that comes in the VW3A1006 remote keypad kit?

Product Line:
VW3A1006

Environment:
All 

Cause:
Needs to replace the mounting screws

Resolution:
M3x10 thread forming screws are used on VW3A1006 remote keypad kit. 
Was this helpful?
What can we do to improve the information ?