Technical FAQs

Ask a Question

What is the altitude derating of the iC60 circuit breakers?

The iC60 circuit breakers from the Acti9 range can be installed in altitude in accordance with the parameters listed in the following table:
Was this helpful?
What can we do to improve the information ?