Technical FAQs

Ask a Question

Is the C60PV-DC compatible with the RCA remote control module?

No, the C60PV-DC is not compatible with the RCA remote control module. For the C60PV-DC there is no possibility for remote closing. Remote opening can be achieved with an MX shunt trip.
Was this helpful?
What can we do to improve the information ?