Technical FAQs

Ask a Question

Osisense XC special - Chain & chain sprocket of the XR2AB10K* : repair issue of the accessories

A customer changed some screw limit switch XR2AB10K*, having a chain sprocket XR2AZ216 and a chain 12.7 pitch. It changed only the chain sprocket and had the following issue after repair: the new sprocket does not match to the old chain (see attached pictures). The solution to solve such issue is to replace both accessories together (see the third picture showing new accessories).

 
Was this helpful?
What can we do to improve the information ?