Technical FAQs

Ask a Question

Which comb busbar is compatible with the Acti9 STI and SBI types of fuse holders?

With the STI type of fuse carriers the comb busbars with the following reference numbers are compatible: 14881, 14880, 14882, 14883, 14884. The choice depends on the fuse carrier's number of poles.

For the SBI type fuse holders we don't have in our offer a compatible busbar, due to the product's different design.
Was this helpful?
What can we do to improve the information ?