Technical FAQs

Ask a Question

Access to the path 'Data' is denied

Issue
The following error occurs when the user tries to select a path to save the archive file:

          
          The following error occurred:
          Access to the path 'Data' is denied.



Product Line
Power Monitoring Expert, PME (all versions)

Environment
Database Manager

Cause
Database Manager is opened by running the executable in .../System/Bin folder.

Resolution
The executable needs to be run with administrative privilege.  Right click on the executable and select 'Run as administrator'.
Was this helpful?
What can we do to improve the information ?