Technical FAQs

Ask a Question

How do I set the low speed for my speed reference on ATV320 drive? 

Issue:
ATV320 How do I set Low speed for my speed reference? 

Product Line:
ATV320 

Environment:
All Serial numbers

Cause: 
No External speed reference

Resolution: 
Goto DRI- > CONF > FULL > SIM 
LSP [Low speed]   
Motor frequency at minimum reference, can be set between 0 and [High speed] (HSP).
See [Low speed] (LSP)
 
Was this helpful?
What can we do to improve the information ?