Technical FAQs

Ask a Question

Is Canalis KS range suitable to be used in a network with the rated voltage 200 V Ph-Ph ?

Yes, the Canalis KS range can be used without restrictions on a network with rated voltage 200V Ph-Ph.
Was this helpful?
What can we do to improve the information ?