Technical FAQs

Ask a Question

Is STBNCO2212 complies with the ISO 11898-2 CANopen Standard?

STB use IXXAT for CANopen and is able to support up to 1Mbps communication as slave, so it should comply with ISO11898-2 standard.
Was this helpful?
What can we do to improve the information ?