Browse FAQs

Padlocking facility in INF Fupact

Published date: 11 September 2018

To padlock the INF switch-disconnector fuses in ON or OFF position,the standard handles (Direct or Extended) can be fitted with 2 or 3 padlocks (not supplied).
Locking in the OFF (O) position ensures isolation complying with standard IEC 60947-3.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.