Technical FAQs

Ask a Question

Osisense XS - Cross-reference of the obsolete XS1N08PA349D inductive sensor

The obsolete XS1N08PA349D proximity sensor can be replaced by the XS108B3PAM12 inductive sensor, since 2013. Attached both data sheets for comparison. The nominal sensing distance Sn of the suggested reference is a little bit shorter (2mm instead of 2.5mm)
Was this helpful?
What can we do to improve the information ?