Browse FAQs

How do you memory protect the M340 CPU?

Published date: 30 September 2019

The M340 can be placed into memory protect by designating a discrete input in the M340 configuration. The input that you designate must exist and must be hard wired
to allow a toggle between 0>1 or 1>0 for memory protect to be turned off and on. Use only topological references for the memory protect input.


Legacy KB System (APS) Data: RESL212705 V1.0, Originally authored by RoAl on 10/09/2013, Last Edited by RoAl on 10/09/2013
Related ranges: Modicon M340

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.