Browse FAQs

Can I add an expansion rack to an existing Quantum RIO drop using the CCOTF option?

Published date: 13 September 2019

Issue
Adding an extended rack to RIO drop with CCOTF

Product Line
Modicon Quantum

Resolution
No. It is not possible to add an XBE interface and backplane to an existing Quantum RIO drop using CCOTF.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.