Technical FAQs

Ask a Question

Can the 140DRA840 00 Relay Output wiring be altered so that the potentials on the Output and Common terminals are reversed?

Yes, if the source(s) applied to the module are not grounded a positive potential can be applied to the common terminal and the common can be applied to the output terminal.

Issue: Application

Product Line: Quantum IO

Environment: n/a

Cause: n/a

Resolution: n/a

Was this helpful?
What can we do to improve the information ?