Browse FAQs

Is there a System Word which will tell us the percent of program fragmentation?

Published date: 25 January 2019

No. There is not a %SW which will provide a fragmentation percentage or %S which would indicate the need for a PACK command.
There is an red icon in the form of an SD card that will appear in the lower right of your Unity screen when the need to Pack arises.



R-301017

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.