Technical FAQs

Ask a Question

Is there a System Word which will tell us the percent of program fragmentation?

No. There is not a %SW which will provide a fragmentation percentage or %S which would indicate the need for a PACK command.
There is an red icon in the form of an SD card that will appear in the lower right of your Unity screen when the need to Packarises.

 
Was this helpful?
What can we do to improve the information ?