Browse FAQs

Type of connection terminals in NSXm.

Published date: 06 May 2019

As standard, NSXm circuit breakers are delivered with EverLink lug connectors for bare cables.
They may be delivered with connectors for bars or cables with compression lugs too.
All lug options are field installable. So, no matter which lugs are on the product, they can be removed and replaced by any one of the 4 kinds of lugs available (EverLink lug with control wire terminal, EverLink lug,compression lug/busbar,aluminium mechanical lug)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.