Technical FAQs

Ask a Question

Why are the torque limit settings not showing up in the ATV66 drives test and commissioning software?

Issue:
Why are the torque limit settings not showing up in the ATV66 drives test and commissioning software?

Product Line:
ATV66

Environment:
All 

Cause:
Not in constant torque mode

Resolution:
You have to put the drive in constant torque mode and its type needs to be SVC ( High Torque) before the Torque limit setting will show up.
 
Was this helpful?
What can we do to improve the information ?