Technical FAQs

Ask a Question

How can I access Ecodial Advance calculation tutorial Videos?

Issue: The Video tutorials in the Ecodial software are unable to access. All these video tutorials are linked to SE TV. Unfortunately, SE TV is decommissioned now & because of that users are unable to access those videos.
Impact: The Ecodial tutorial links are directing the users to wrong webpage and videos are not available.
Workaround: With the same tutorial name, please search for the videos in the Youtube.
Example: Find the snapshot below


Note: Till the next version of Ecodial (EAC 4.8.6 INT) release, please use the Youtube links directly.
 
Was this helpful?
What can we do to improve the information ?