Browse FAQs

Osisense XC - Dimensions of the ZCKE235 switch head

Published date: 28 August 2019

The ZCKE235 head reference is the hot version of the ZCKE23, sub-assembly for high temperature up to +120°C. ZCKE235 dimensions are the same as those of the ZCKE23. Hereafter the Traceparts library @ of the ZCKE23 head, valid too for the ZCKE235 (+120°C) or ZCKE236 (-40°C)
https://www.traceparts.com/els/telemecanique-sensors/en/product/telemecanique-sensors-limit-switches-osisense-xc-industrial-metallic-conforming-to-standard-en-50041-type-xckj-sub-assembly-head-steel-roller-lever-plunger-horizontal-actuation?CatalogPath=TELEMECANIQUE_SENSORS%3ATELEMECANIQUE_SENSORS.010&Product=10-22052013-082818&PartNumber=ZCKE23

Attached catalogue dimensions of the ZCKE23 head


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.