Technical FAQs

Ask a Question

How to perform factory reset on an IFM TRV00210 module?

Following the steps below, the IFM module (TRV00210) can be restored to factory settings:
  • Set the X10 and X1 dials to 0
  • Set the locking dial to unlock
  • Press the test button for 1 minute
Was this helpful?
What can we do to improve the information ?