Technical FAQs

Ask a Question

What is the service life time of the Compact NS 100-630 circuit breakers?

The assumed service life of the product is 20 years and the European electrical power model is used.
Detailed information is available in the attached Product Environmental Profile.
Was this helpful?
What can we do to improve the information ?