Technical FAQs

Ask a Question

What is the flammability rating of Compact NSX circuit breakers according to UL94?

The flammability rating of the block and cable base material is:  UL94 Flame Class V-0.
Was this helpful?
What can we do to improve the information ?