Technical FAQs

Ask a Question

What is the maximum tolerance for alignment of two Canalis KT busbars?



In the 2 directions Y and Z from the screen shot above (vertical and horizontal directions), 2mm misalignment is valid whatever the busway's installation position (edgewise or flat wise).

In the X axis, the "length" adjustment during product positioning should manage the gap 40mm with a tolerance of +4mm and -2.5mm (so: from 37.5 to 44mm)

Was this helpful?
What can we do to improve the information ?