Technical FAQs

Ask a Question

What is the quantity of gasket delivered with 1 piece of 88670 or 88671?

1pc 88670 = 10 rolls
1 roll 88670 = 17.7m of 25X8mm gasket
TOTAL: with 1 piece of 88670 reference number ordered, 175m of gasket are delivered.

1pc 88671 = 10 rolls
1 roll 88671 = 20m of 10X6mm gasket
TOTAL: with 1 piece of 88671 reference number ordered, 200m of gasket are delivered.
Was this helpful?
What can we do to improve the information ?