Technical FAQs

Ask a Question

What is the minimum voltage on which the Acti9 RCD / RCCB can be used?

The network's minimum voltage level required for the correct functioning of the Acti 9 RCDs and RCCBs, including the functionality of the Test button is -15% / +10% of Un rated voltage.
Was this helpful?
What can we do to improve the information ?