Osisense XM - Is the XMLP250BD21F pressure transmitter compatible with the triethylamine
1) The triethylamine is an extremely flammable liquid and vapor. In the IEC grouping, it is classified in Group II, A (Class I, Group D) (see attachment). An Atex gas product suitable for such liquid has to be selected.
2) The XMLP250BD21F pressure transmitter is not certified for such Atex use. Alternative is to consult the Ex-tech company at the following @ http://www.ex-tech.no/en/home/